What's New¶
Labeling¶
The Labeling feature enables branding and UI theming customization for WAGO VC Hub during product delivery.
For Labeling, customers first need to provide their branding materials to us. Based on these materials, we will create a customized package and provide a dedicated installation package for specific customers. This feature is mainly intended for system integrators.
Currently, Labeling supports customization of the following items:
- Brand Information
- Images and Logos
- Theme Colors
Labeling is not available during installation or on the onboarding pages.
Password Reset¶
When users forget their passwords, they can reset them in two different ways.
- Reset via email
- Reset using the command-line tool included in the installation package
To reset password via email, you need to configure an email service for password recovery and set an email address to the user account.
To reset a password using the command-line tool, the tool must be run with administrator or root privileges.
Separate licensing for runtime and engineering users¶
The user type have been added for users,including Engineering User and Runtime User.
When a user logs in, the system opens the corresponding interface based on the assigned user type.
-
After logging in, Engineering Users are redirected to the Admin Console page, where they can perform system configuration and access design-related pages.
-
After logging in, Runtime Users are directed to the runtime pages for system monitoring and operation.
Users with security permissions can view all currently online engineering and runtime users under the Security → Online User menu. They also have the ability to force log out selected users.
IEC 60870-5-104¶
The system now includes support for the IEC 60870-5-104 (IEC 104) communication protocol, enabling VC Hub to communicate efficiently and reliably with industry-standard power equipment and dispatching systems, and providing real-time monitoring and remote control capabilities while enhancing system interoperability and industry compatibility.
Add New License Items¶
- Added a license item for 100,000 I/O tags
- Added a license item for IEC 104
- Added a license item for 20 Engineering Concurrent Online Users and 200 Runtime Concurrent Online Users
- Added a license item for 50 Engineering Concurrent Online Users and 500 Runtime Concurrent Online Users
Concurrent Online Users Include Engineering Users and Runtime Users¶
Increased the number of runtime concurrent users based on the existing concurrent online user count.
| Original Logic | New Logic |
|---|---|
| 1 concurrent online user | 1 engineering user and 10 runtime users |
| 2 concurrent online users | 2 engineering users and 20 runtime users |
| 5 concurrent online users | 5 engineering users and 50 runtime users |
| 10 concurrent online users | 10 engineering users and 100 runtime users |
| 20 concurrent online users | 20 engineering users and 200 runtime users |
| 50 concurrent online users | 50 engineering users and 500 runtime users |
OPEN APIs Enhancement¶
This release significantly enhances the OpenAPI capabilities.
It introduces batch and CRUD (create, read, update, delete) APIs for assets, models, instances, tags, and alarm configurations, along with improved metadata support such as extended attributes and the ability to retrieve full tag information in a single response. Error messages have also been improved to provide clearer and more consistent feedback.
In addition, full lifecycle management APIs are provided for Modbus TCP devices and frames, including creation, modification, deletion, start/stop control, connection status subscription, connection testing, and device querying with frame information.
Two New Navigation Types Added to the Menu Control¶
When clicking a menu item in the Menu control, in addition to the existing options of navigating to a new page or opening a new popup window, two new navigation types have been added: Page Container and IFrame.
Within a Page Container or IFrame, users can now switch between different pages by clicking menu items without refreshing the current page.

Support importing projects across minor versions¶
Projects can be imported from an earlier minor version into a later minor version, such as from 5.0.x to 5.1.x. Previously, only projects from the previous patch version, such as 5.0.1 to 5.0.2, were supported.