Skip to content

User Interface Overview

Top Bar Functions

The top area of the MEMS user interface provides three main categories of functions:

1.Message Notifications

2.Version Information

3.System Login

alt text

1. Message Notifications

Message notifications indicate normal system events, successful operations, or automatic regulation activities, generally divided into three categories based on severity and display color:

alt text

Color Severity Meaning Typical Operator Action
Yellow Warning A potential issue or abnormal condition that requires attention. Monitor the condition and take preventive action if necessary.
Red Error / Critical A fault, failure, or critical condition that may affect system operation. Immediate action is required. Follow the alarm handling procedure.
Black Info A normal event, status change, or successful operation. No immediate action is required. Review if necessary.

The following action will trigger info message on black icon:

  1. VC Hub is successfully connected

  2. Sync is started or completed

  3. System trigger Peakload regulation

  4. System trigger Avoid Peakload regulation

  5. System trigger Reactivation regulation

  6. System stop Reactivation regulation

The following action will trigger Error / Critical message on red icon:

  1. VC Hub is disconnected

  2. License expired

The following action will trigger Warning message on yellow icon:

  1. Sync failed

  2. No License is available

  3. License almost expired

  4. Surplus regulation failed

The count of unread messages is displayed at the top of the icon. Click the icon, and detailed messages will be shown in the list.

Click the 'Mark all read' button, and the system will automatically mark all unread messages as read; the number of unread messages will decrease to 0.

Click the 'Clear all' button, and the system will automatically delete all messages in the list.

alt text

Error / Critical messages cannot be removed from the notification list until the user has explicitly acknowledged them. This prevents critical events from being missed, ignored, or deleted without review.

alt text

alt text

alt text

When all Error / Critical or Warning messages are cleared, the relevant icon will disappear.

alt text

2.Version Information

Click the Version Information button, and the Version Information will be displayed.

alt text

alt text

3.System Login

The user avatar in the top bar provides access to account-related functions. Clicking the avatar will display detailed user information. Clicking the Logout button allows the user to securely log out of the system.

alt text

SiderBar Functions

MEMS provides an integrated set of functions for configuring, monitoring, controlling, and reporting on microgrid operations. It supports the full workflow from component creation and data connection to automatic regulation, alarm handling, system configuration, and energy reporting. Users can perform these actions by clicking the sidebar buttons.

alt text

1.Dashboard

The Dashboard provides a centralized overview of energy usage across the system. It summarizes how energy is generated, consumed, stored, and exchanged, allowing users to quickly assess the current operating condition of the site.

alt text

'Energy Overview' displays an overview of energy usage for all configured endpoints and allows users to configure consumption endpoints and generation endpoints in VC Hub.

'System State' detects abnormal conditions based on Load Management Settings or user-defined alarms and displays the corresponding system status.

'Current Alarm' can display user-defined alarms when the configured alarm conditions are triggered.

2.Microgrid Components

The Microgrid Components page allows users to build and manage the logical structure of the microgrid by adding different components, subgroups, or folders.

alt text

alt text

alt text

alt text

Users can create different types of components and synchronize them to VC Hub.

alt text

Once synchronized and connected to real data sources, component data becomes available on the component details page.

alt text

alt text

3.Constraints & Tasks

The Constraints & Tasks page allows users to define time-based Constraints and Tasks, as well as scheduled actions for the microgrid.

Constraints limit how the system or a component may operate during a specified period. Tasks can schedule the charging of a battery component during a specified period.

alt text

4.Peak Load Management

Peak Load Management is a control and monitoring function that helps maintain grid power and site consumption within a configured range. It provides two main capabilities:

  1. Display system energy changes — visualize how generation, consumption, storage, and grid exchange vary over time.

    alt text

  2. Adjust system consumption — automatically regulate consumption when it is too high or too low, keeping operation within the configured reasonable range by using created stages.

    alt text

This function supports peak shaving, demand charge reduction, grid stability, and efficient use of renewable generation and battery storage.

5.Alarms

The Alarm interface provides a centralized view of all alarms generated in the system. It displays two main categories of alarms:

  1. Regulation-triggered alarms — alarms generated automatically by the system during regulation actions, such as peak load management, battery control, or surplus handling.

  2. User-defined alarms — alarms generated when a condition configured by the user is met, such as a threshold, anomaly, or custom event.

alt text

The Alarm interface helps users monitor system health, respond to abnormal conditions, and review historical events.

6.Reporting

The Reporting interface provides users with a clear view of energy consumption over time. It supports both annual and monthly consumption views, allowing users to analyze trends, compare periods, and support energy management decisions.

alt text

The range of data that users can see is controlled by configuration in the Project Settings page. Only data within the configured visibility range will be displayed in reports.

alt text

7.Project Settings

The Project Settings page provides system-level configuration options for the MEMS project. It allows authorized users to define basic project information, control time and regional settings, enable or disable load management, manage data retention, configure licensing, and verify connectivity to VcHub.

This page typically includes the following configuration areas:

  1. Modify Project Information, set System Time Zone

    alt text

  2. Set Load Management Settings

    alt text

  3. Set Data Storage Limitation

    alt text

  4. License Configuration

    alt text

  5. VC Hub Connection Test

    alt text