Skip to content

User Attribute Mapping

User attribute mapping allows you to map information from the Identity Provider response document to easily understandable attributes. For this to work, VC Hub must already have a valid Identity Provider configuration that returns a response document when attempting to log in.

Configuring User Attribute Mapping

  1. Click the "Security" → "Identity Provider" menu.
    alt text
  2. In the Identity Provider list, click the "User Attribute Mapping" for a specific entry in the action column. alt text
  3. In the pop-up window, set the source and mapping path. The system provides the following 5 properties that can be used for mapping: alt text

Notes:

  • The User Attribute Mapping option is only available when the data type is OpenID Connect.

Properties

Name Description
Username Mapping for username.
Role Mapping for role.
Name Mapping for name.
Email Mapping for email.
Phone Mapping for phone.
Source The mapping includes the following:
- ID Token Claims: These are the claims in the ID token used to represent the user's identity information. They typically include attributes like, name, email, etc.
- Token Endpoint Response: This is the response from the token endpoint, which typically includes the Access Token, ID Token, and Refresh Token. These tokens are used to authenticate and authorize the user.
- User Info Claims: These claims contain detailed user attributes such as name, email, profile picture, and other personal information. These are usually returned by the Identity Provider when querying the UserInfo Endpoint.
Mapping Path It is typically used to map the user information returned by the Identity Provider to the local system's user model, ensuring that the application can correctly identify and authorize the user.

4.Click the "OK" button to complete the setup.

Example

  1. Assume the ID Token returned by the Identity Provider contains the following information:

{

"username": "alex",

"email": [email protected],

"user_roles": "admin"

"name": "Alex Zhang"

}

2.The mapping paths can be set as follows:

alt text

  • username → The local username(username)
  • email → The local email(email)
  • user_roles → The local role(role)
  • name → The local name(name)

3.In VC Hub, the end-user information is mapped as follows:

{

"username": "alex",

"email": [email protected],

"role": "admin"

"name": "Alex Zhang"

}