Skip to content

Subscribe to real-time data

Open API offers WebSocket API for real-time data access.

Using the WebSocket API, you can subscribe to real-time data, including tag values, tag properties, and tag alarms.

  1. Open the postman home page, click the + icon, then click the View more templates link.

    alt text

  2. Click the API protocol 101 menu, then select the WebSocket basics option.

    alt text

  3. Create a new folder under WebSocket basics Open the menu by clicking the dropdown menu of the new folder, as shown in below screenshot, then click the WebSocket option.

    alt text

  4. Enter ther URL wss://localhost:8043/ws/v1/realtimeData

    alt text

  5. Open the Params tab and enter the access_token.

    alt text

  6. Click the Connect button, and Postman will indicate the Websocket connection has been established.

    alt text

  7. Once connected, open the Message tab and send payload with the format like the below example. Note that the special charactar alt text must not be ignored. The part [["Default:m1","Default:m2","Default:m3"]] in third line should be replaced the tags actually exist in the system.

    {"protocol":"json","version":1}alt text

    {"type":6}alt text

    {"arguments":[["Default:m1","Default:m2","Default:m3"]],"invocationId":"0","target":"TagValues","type":4}alt text

    alt text

8.After the payload is sent, postman will continuously receive the real-time tag values. alt text

9.The above example demonatrates how to subscribe the tag values. For the other Websocket APIs, refer to chapter Realtime Data API Definitions. The target field in the payload in the example below represents the method name of Reamtime Data API. You can call the other WebSocket APIs by replacing target value with the method name specified in the Realtime Data API Definitions document. alt text