WAGO Protocol¶
The WAGO Protocol driver in VC Hub supports the basic connection to WAGO PLCs. The system comes with an MQTT Broker, which supports the user's connection via the account and password provided by the system and the data communication via the WAGO Protocol driver.
Supports WAGO Protocol version 1.5.0.
Driver Connection to WAGO Protocol¶
- On the "Devices" -> "WAGO Protocol" screen, click the "Add" button.
- Enter the device name in the Add window.

- Click on the "OK" button. The data will now be displayed in the device list of the WAGO Protocol. Please note that the status column only indicates the start/stop status of the driver, not the actual connection status of the device.

Configuration Fields
| Name | Description |
|---|---|
| Device Name | Device name, unique in the device list. |
| User Name | Account number used to connect with a certain device, automatically generated by the system, cannot be modified. |
| Password | Password used to connect with a certain device, automatically generated by the system, supports reset. |
Note:
- Please keep your username and password information in a safe place to avoid leakage to unauthorized personnel, and if leakage occurs, please reset your password in time.
- Enable All and Disable All are to enable or disable all data in the list.
Connecting to the System MQTT Broker¶
Before you can use the WAGO Protocol driver, you need to connect to the MQTT Borker, please follow the steps below to do so:
- Get account and password: Click on the "View" button of the device to see the user name and password provided by the system.
-
Configuration of Cloud Connectivity
- Use a web browser to open the WBM (Web-based Management) of your WAGO device.
- Enter the Username and Password to authenticate on the PFC, then click Submit.
- Under Configuration, select the Cloud Connectivity menu item and click on Connection1.
- In the configuration section on the right, check the Enabled box to enable the current connection.
- From the Cloud platform drop-down list, select MQTT AnyCloud.
- In the Hostname field, enter the IP address published by your VC Hub program.
- In the Port field, enter 1884.
- In the Client ID field, enter the device identifier, which must match the device name added in the WAGO Protocol device list. This is used to identify your connection on the MQTT Server.
- Check the Clean session box to enable session clearing.
- In the User field, enter the username for connecting to the MQTT Server, using the username from the device information added in the WAGO Protocol device list.
- In the Password field, enter the password for connecting to the MQTT Server, using the password from the device information added in the WAGO Protocol device list.
- From the Data protocol drop-down list, select WAGO Protocol 1.5.
- Click Submit and restart the device.
- After a short wait, check the connection status in Cloud Connectivity on the WBM. The Cloud connection will display "connected".
- There is no need to configure other options, as the current VC Hub program does not implement them.
Note: Please do not check Use Compression, as this will cause the WAGO Protocol driver to fail in processing data. And for the fields not mentioned in the above list, checking these fields does not affect functionality, because VC Hub has not yet implemented the corresponding features.
3. Connect to MQTT Broker: After confirming a successful connection, you can start transferring device data with the WAGO Protocol driver using the configured client.
Enabling TLS Secure Connections¶
The VC Hub program supports a secure connection with WAGO PLC devices via the TLS protocol.
Configure the client: Modify the connection configuration in the configuration page of the WAGO PLC device.
- Port number: Change to 3883.
- TLS: Select Enabled.
- CA File: Fill in the path, /etc/ssl/certs/ server-cert.pem.
- Obtain server certificate: Log in to the PLC system and execute commands: openssl s_client -connect [server IP] :3883-showcerts /dev/null | openssl x509 -outform PEM > /etc/ssl/certs/server-cert.pem
Note: Replace [server IP] with the server IP deployed by VC Hub.

Publishing and subscribing to device data¶
Refer to the WAGO Messaging Protocol , official documentation at https://www.wago.com/us/d/15719.
Binding to tags¶
Bind a tag to a client measurement point.
- Create an I/O tag.

- On the add window, click the binding button of the data source.

- Select the points to be bound.

- Click the "OK" button to complete the configuration.