Database Table Reference¶
VC Hub integrates multiple built-in systems that automatically query data without requiring manual construction of query logic or table structures. These systems autonomously create necessary tables in the database, insert relevant data, and provide appropriate querying methods.
Since historical data is stored within database tables, users have the option to manually access and query the data, enabling customized data views as needed.
Notes
These tables follow specific structural definitions. Unintended modifications to table structures may lead to unpredictable issues. It is strongly advised not to alter or delete existing table structures.
Although direct manual querying of table data is technically possible, we recommend performing a full database backup prior to making any changes or executing operations. Please note that any risks resulting from modifications to data or table structure will be the responsibility of the user.
VC Hub supports both traditional relational databases and the time-series database InfluxDB. As a result, table structure definitions vary depending on the type of database in use.
- Relational databases share a unified set of table definitions.
- InfluxDB employs a separate and distinct schema structure.
Introduce¶
Before introducing the table structures, it is essential to understand the relevant foundational configurations. These preliminary settings serve as the groundwork for proper database operation and ensure seamless integration with VC Hub’s data management systems.
Node¶
VC Hub includes a node configuration feature, where the node name is by default set to the server’s hostname. Users may modify this name to suit their operational needs.
The node primarily serves as a unique identifier, enabling other VC Hub instances within the network to easily recognize and communicate with it. When historical data is stored, the system also records the name of the node responsible for the data storage process.

Asset¶
On the "Tags → Asset" page, you can configure the historical storage for tags. When "History" is enabled for a tag, its historical data will be stored in the corresponding history database.

History Database¶
On the "Database → History Database" page, you can configure the storage medium and storage format for tag history data.

Database Connection¶
The VC Hub system currently supports five types of databases: MySQL, SQL Server, PostgreSQL, SQLite, and InfluxDB.
Users can configure the database connection by specifying the appropriate connection URL, username, and other relevant credentials. These configured databases are then utilized for storing alarm history and tag history data.