Skip to content

SQLite

On this page, we will demonstrate how to connect VC Hub to SQLite.

  1. On the "Databases" -> "Database Connection" page, click the "Add" button. alt text
  2. In the following pop-up window, select SQLite and click the Next button. alt text
  3. Enter the following information in the configuration interface (Note: The following data is only an example, please fill in according to the actual situation).

    Since SQLite is an open source embedded relational database that implements a self-contained, serverless, configuration-less, transactional SQL database engine. It is a zero-configuration database.

    So creating a SQLite database connection means creating a SQLite file locally. So there is no need for Host, Port, Username, Password, etc. You just need to check where the SQLite file is stored.

    alt text

    • Name: Demo
    • Storage Path: {WorkspaceDirectoy}/database/history
    • Database name: history
    • Connection timeout(ms): 10000
    • Maximum Query Points:1000000
    • Query Timeout(s):30

    Notes:

    1. The database name is the name of the SQLite file without suffix.

    2. The storage path of SQLite file supports placeholders such as"{WorkspaceDirectory}/database/history". This allows users to create a history database file within workspace folder by utilizing the placeholder in the storage path.

  4. Click "OK" button, the popup window will be closed and the list of database connections will be displayed. The connection status of the data in the list is "Connected". alt text