Skip to content

SMS(Ali Cloud)

This configuration is used to define what is included in the SMS notification sent via Ali Cloud when an alarm is triggered.

Create Notification Content SMS(Ali Cloud)

  1. Click "Alarming"->" Alarm Notifications "->" Messages" to enter the notification message list page. alt text
  2. Click the "Add" button. In the new pop-up window, select "SMS(Ali Cloud)". alt text
  3. Click "Next" to enter the detailed configuration window. alt text
  4. Once the setup is complete, click "Send Test" to check if the sms is sent successfully.
  5. If the test is successful, click the "OK" button to add the data.

Properties

Name Description
Name The name of the notification message is required. The name is unique and cannot be repeated.-
Description The subject of the email received. -
Sign Name The signature name successfully applied for in the Ali Cloud SMS service.
alt text
Template Code The template code successfully applied for in Ali Cloud SMS Template Code.
alt text
Send Test After the above configuration, click the 'Send Test' button and a new window will pop up. Enter the mobile phone number for receiving the test SMS in the new window, select the SMS service that has been created, and click the 'Send' button to check whether the SMS can be received correctly.
alt text

How to use the Ali Cloud Notification Service

In the alarm notification rules, you will select the notification service.

  1. Click on "Alarming" -> "Alarm Notifications" -> "Rules" to enter the notification rules list page.
  2. Click the "New" button in the upper right corner of the list.
  3. In the pop-up window, click the '+SMS' button to add a new sms notification rule.In the notification message dropdown, select the previously created notification message.

    alt text

Note: Notification content and notification service must match. For example, when you select the notification service for SMS(Ali Cloud), you should also select SMS(Ali Cloud) as the notification message.