Skip to content

Installation and Upgrade

Installation Environment

VC Hub provides installation packages for both Windows and Linux environments. VC Hub does not support container deployment. Do not run it in a container.

If an old version is already installed in the installation environment, please uninstall it first. VC Hub does not support upgrade installation. You must uninstall the installed version before each new installation.

Note: Please close all local anti-virus software before installation. Because some antivirus software may mistakenly identify the installation files as viruses.

Ports

The installation program defaults to using port 8066 for HTTP and port 10443 for HTTPS. Please ensure that port 8066 is available during installation.

Port Description Configuration
8066 HTTP default port "Node">"Node Settings">"Web Server"
10443 HTTPS default port "Node">"Node Settings">"Web Server"
8099 Networking default port "Node">"Networking">"Main"
1883 Built-in Mqtt Broker default TCP port "Node">"MQTT Broker">"Basic"
8883 Built-in Mqtt Broker default TLS port "Node">"MQTT Broker">"Basic"

The http and https ports are configured as follows:

alt text

The networking port is configured as follows:

alt text

The Mqtt port is configured as follows:

alt text

Version

VC Hub uses a version structure: "Major Version. Minor Version. Revision Version". The project data version must match the version of the running program to operate.

Uninstallation

The user data directory and the installation program directory are independent. Uninstalling will not delete user data. If necessary, you can manually delete the user data directory.

Upgrade

Direct upgrade installation is not currently supported. Before upgrading, please uninstall first. After uninstalling, install the new version.

System Environment Tags

Tag Name Description Windows Environment DefaultValue Linux Environment DefaultValue Usage Instructions
WAGO_Visualization_And
_Control_Hub_APP
Installation directory C:\Program Files\WAGO Visualization And Control Hub /usr/local/bin Used only to record the application directory, do not modify.
WAGO_Visualization_And
_Control_Hub_DATA
Data directory C:\ProgramData\WAGO
VisualizationAndControlHub
/usr/share/wagovisualization
andcontrolhub
Used to configure the VC Hub application data directory.
If not configured, the default value is used.
If you want to change the application directory, you can modify this tag value and restart the application for the configuration to take effect.
WAGO_Visualization_And
_Control_Hub_Version
Version Installation program version Installation program version Used only to record the application version, do not modify.

User Data Directory

Windows installation environment user data directory: "%ProgramData%\WAGOVisualizationAndControlHub", usually "C:\ProgramData\WAGOVisualizationAndControlHub".

Linux installation environment user data directory: /usr/share/wagovisualizationandcontrolhub

Restart Service

Windows environment: Restart the VC Hub service in the system services.

alt text

Linux environment: sudo systemctl restart virtualiztionandcontrolhub

And you can also stop the service first: sudo systemctl stop virtualiztionandcontrolhub and then start the service: sudo systemctl start virtualiztionandcontrolhub