Skip to content

System.Tag.readHistory

Description

Retrieve the historical records of the current tag, including the tag's path, value, quality code, time and aggregation mode.

Grammar

enum AggregationMode { "Raw", "Avg", "Max", "Min", "First", "Last", "Count", "Range", "CountOn", "CountOff", "DurationOn", "DurationOff" }

enum PeriodMode { "Second", "Minute", "Hour", "Day" }

interface ExtraOption { 
  timeout?: number; 
  noInterpolation?: boolean;
  ignoreBadQuality?: boolean; 
  includeBoundingValues?: boolean 
}

interface TagHistoryData {
  path: string;
  value: any;
  quality: string;
  time: string;
  aggregationMode: AggregationMode;
}

System.Tag.readHistory(
  start: Date | string,
  end: Date | string,
  tag: string | Array<string>,
  queryMode: "Raw",
  extraOption?: ExtraOption
): Promise<Array<TagHistoryData>>;

System.Tag.readHistory(
  start: Date | string,
  end: Date | string,
  tag: string | Array<string>,
  queryMode: "FixedPoints",
  aggregationMode: AggregationMode | Array<AggregationMode>,
  points: number,
  extraOption?: ExtraOption
): Promise<Array<TagHistoryData>>;

System.Tag.readHistory(
  startDate: string | Date,
  endDate: string | Date,
  tag: string | Array<string>,
  queryMode: "Periodic",
  aggregationMode: AggregationMode | Array<AggregationMode>,
  period: number,
  periodMode: PeriodMode,
  extraOption?: ExtraOption
): Promise<Array<TagHistoryData>>;
Parameter

Name Type Description
start Date or string Start Time
end Date or string End Time
tag string or Array<string> Tag(s) to query
queryMode QueryMode Query Mode
aggregationMode AggregationMode or Array<AggregationMode> Aggregation mode(s) required for "FixedPoints" and "Periodic" query modes
points number Points,required for "FixedPoints" query modes
period number Period,required for "Periodic" query
periodMode PeriodMode Period mode,required for "Periodic" query modes
extraOption.timeout number The timeout duration for the query, measured in seconds
extraOption.noInterpolation boolean Interpolation enabled? (true to disable)
extraOption.ignoreBadQuality boolean Ignore bad quality samples in data query
extraOption.includeBoundingValues boolean Whether to include bounding values during interpolation. If there is no data at the start or end of the query time range, the system will retrieve the last value within one day before the start, and the first value within one day after the end, for interpolation

Code Example

Retrieve the historical records of the raw values for the tag "Device:Temperature" between 2024-08-14 00:00:00 and 2024-08-15 00:00:00.

const value = await System.Tag.readHistory('2024-08-14 00:00:00', '2024-08-15 00:00:00', '@Device:Temperature','Raw',{
  timeout: 30
});
console.log(value);
Retrieve the historical records of the variable "Device:Temperature" between 2024-08-14 00:00:00 and 2024-08-15 00:00:00 using the "FixedPoints" query mode, with "Avg" as the aggregation mode and a total of 30 data points.

const value = await System.Tag.readHistory('2024-08-14 00:00:00', '2024-08-15 00:00:00', '@Device:Temperature','FixedPoints','Avg',30, {
  timeout: 60,
  noInterpolation: true,
  ignoreBadQuality: true,
  includeBoundingValues: false
});
console.log(value);
Retrieve the historical records of the variable "Device:Temperature" between 2024-08-14 00:00:00 and 2024-08-15 00:00:00, using the "Periodic" query mode, with "Max" as the aggregation mode, a period of 1, and "Minute" as the period mode.

const value = await System.Tag.readHistory('2024-08-14 00:00:00', '2024-08-15 00:00:00', '@Device:Temperature','Periodic','Max',1,'Minute', {
  timeout: 60,
  noInterpolation: true,
  ignoreBadQuality: true,
  includeBoundingValues: false
});
console.log(value);