System.Alarm.queryHistory¶
Description¶
Query the historical alarms of the current historical storage.
Grammar¶
System.Alarm.queryHistory(historyStorage:string): Promise<any>
System.Alarm.queryHistory(historyStorage:string,params:{
startTime?: Date | string,
endTime?: Date | string,
priority?: AssetAlarmPriority | AssetAlarmPriority[],
state?: AssetAlarmState | AssetAlarmState[],
path?: string | string[],
type?: AssetAlarmType | AssetAlarmType[],
asset?: string | string[],
expression?: string}): Promise<any>
- Parameter
historyStorage - Name of the history storage
params - The query conditions object, optional parameters
{
startTime? - Start time, default is 8 hours before the current time
endTime? - End time, default is the current time
priority? - Priority(s), optional values are "Low","Medium","High","Critical"
state? - State(s), optional values are "Active","Unacked","Acked","Cleared"
path? - Alarm path(s)
type? - Type(s), optional values are "H","H2","H3","H4","L","L2","L3","L4","RateOfChange","Equivalent","TrueToFalse","FalseToTrue"
asset? - Asset(s)
expression? - Expression, Example1:priority == "Low", Example2:path.Contains("Device"), Example3:state.HasFlag("Active") && state.HasFlag("Unacked")
}
- Return
[
{
path: string // Alarm path
name: string // Alarm name
type: string // Type
priority: string // Priority
eventId: string // State change ID
eventTime: string // State change time
state: string // State
operator: string // Acknowledgment operator
valueType: string // Value type
value: string // Alarm value
ackTime: string // Acknowledgment time
ackNotes: string // Acknowledgment notes
ackMode: string // Acknowledgment mode
nodeName: string // Node name
storageName: string // History storage name
description: string // Description
},
...
]
Code Example¶
Query the historical alarms from the "Default" historical storage for the past 8 hours.
Query the historical alarms from the "Default" historical storage within the time range from 2025-03-10 00:00:00 to 2025-03-11 00:00:00, with an alarm level of High, a type of H or H2, and a status of "Active, Unacked".