Skip to content

System.Alarm.query

Description

Query real-time alarms.

Grammar

System.Alarm.query(): Promise<any>
System.Alarm.query(params?:{
priority?: AlarmPriority | AlarmPriority[],
state?: AlarmState | AlarmState[],
path?: string | string[],
type?:AlarmType | AlarmType[],
asset?: string | string[],
group?: string | string[],
expression?: string}): Promise<any>

- Parameter
params - The query conditions object, optional parameters
{
priority? - Priority(s), optional values are "Low","Medium","High","Critical"
state? - State(s), optional values are "Active","Unacked","Acked","Cleared"
path? - Alarm path(s)
type? - Type(s), optional values are "H","H2","H3","H4","L","L2","L3","L4","RateOfChange","Equivalent","TrueToFalse","FalseToTrue"
group? - Alarm group(s)
asset? - Asset(s)
expression? - Expression, Example1:priority == "Low", Example2:path.Contains("Device"), Example3:state.HasFlag("Active") && state.HasFlag("Unacked")
}
- Return
[
{
path: string // Alarm path
name: string // Alarm name
type: string // Type
priority: string // Priority
eventTime: string // State change time
state: string // State
operator: string // Acknowledgment operator
valueType: string // Value type
value: string // Alarm value
ackTime: string // Acknowledgment time
ackNotes: string // Acknowledgment notes
recoveryTime:string // Recovery time description: string //
Description ackMode: string // Acknowledgment mode
ruleName: string // Notification Rule groupNames: string // Alarm group
activeTime: string // Activation time
},
...
]

Code Example

Query all real-time alarms.

const value = await System.Alarm.query();
console.log(value);
Query real-time alarms with an alarm level of High, a type of H or H2, an alarm group of Default, and a status of "Active, Unacked".

const value = await System.Alarm.query({priority:"High",type:["H","H2"],group:'Default',expression:
'state.HasFlag("Active") && state.HasFlag("Unacked")'});
console.log(value);