Animation¶
By rationally applying animation effects, VC Hub can bring users a more efficient, intuitive and pleasant interface interaction experience.
In VC Hub, when the model has animation attributes, the "Animation" column will be displayed in the attribute bar on the right. Click the setting button to set the animation.

Value can be configured as either a static value or a binding.Through binding, the enabled state of the animation can change dynamically based on the value of a tag or expression, rather than being manually fixed to "enabled" or "disabled".
Static value:

Binding:
After binding is completed, the binding information can be viewed by clicking the icon.

Animation type¶
VC Hub's 3D models support the following animation types:
Blink¶
The blink effect is easy to attract attention and is often used to alarm when abnormal conditions occur.
Example
Create a sphere model that represents an alarm light that flashes when the value of Temperature is greater than 40.


| Name | Value |
|---|---|
| Enable | Enable |
| Bool value | Expression: tag('@Default:temperature) > 40; Note: This animation only takes effect when the value is a Boolean value. |
| Executions | The number of times to flash when the value is true |
| Duration | The execution time of each flash, unit ms. |
Translocation¶
Let the model perform dynamic effects of displacement through paths.
Example
The model is displaced according to the path on the conveyor belt.

| Name | Value |
|---|---|
| Enable | Enable |
| Duration (ms) | The time for each displacement execution, unit ms |
| Executions | The number of times it needs to be executed when the value is true |
| Reverse Play | Does the model move to the end of the path and then move back in the opposite direction? |
| Face Forward | The model always faces the direction of motion. |
| Path | The path where the model needs to be displaced |
| Bool value | True |
| The world position of current object | Show the world position of current object |
Rotation¶
Use a static value to simulate the rotation of the fan blade.


| Name | Value |
|---|---|
| Enabled | Enable |
| value | True |
| Type | The result type of the value. Divided into Number type and Bool type. Number type: Bool type: ![]() |
| Min Value | When the type is number, this parameter is displayed. Used in combination with the "angle" . Set the min value at which the animation takes effect, and the rotation angle of the model at the min value. ![]() |
| Max Value | When the type is number, this parameter is displayed. Used in combination with the "angle" . Set the max value at which the animation takes effect, and the rotation angle of the model at the max value. ![]() |
| X Axis Offset | The offset of the rotation center along the X-axis relative to its parent. |
| Y Axis Offset | The offset of the rotation center along the Y-axis relative to its parent. |
| Z Axis Offset | The offset of the rotation center along the Z-axis relative to its parent. |
| Direction | When the type is Bool, this parameter is displayed. Indicates the direction of rotation. |
| Rotation Angle | When the type is Bool, this parameter is displayed. Indicates how many degrees to rotate. |
| Executions | When the type is Bool, this parameter is displayed. Indicates how many times it needs to be rotated. |
| Duration(ms) | When the type is Bool, this parameter is displayed. Indicates the duration of each spin. |
| Reverse Play | When the type is Bool, this parameter is displayed. Indicates whether to reversely rotate back after rotating to a specified angle. |
Scale¶
Change the model through changes in values.
Example
The cube determines whether to scale based on a Bool value.



| Name | Value |
|---|---|
| Enabled | Enable |
| Bool value | Tag: Default:Roll Note: This animation only takes effect when the value is a Bool value. |
| Percentage | The size of the deformation of the model. |
| Direction | In which direction the model should deform. |
| Executions | The number of times it needs to be executed when the value is true. |
| Duration | The duration of each deformation, unit is ms. |
| Reverse Play | Indicates whether to scale back after scaling to a specified percentage. |