Update Query¶
Example¶
Add new data to the database.
Steps¶
Creating a database connection¶
On the "Databases"->"Database Connection" page, create a new database connection named TestSQLQuery.

There is a table named person_management in the database, which is used to store personnel information. Its structure is as follows:
| Id | name | gender | age | |
|---|---|---|---|---|
| 1 | Alice Johnson | [email protected] | Female | 18 |
| 2 | Bob Smith | [email protected] | Male | 19 |
| 3 | Charlie Brown | [email protected] | Male | 19 |
| 4 | Diana White | [email protected] | Female | 18 |
| 5 | Edward Green | [email protected] | Female | 20 |
Create SQL Query¶
- Create the project, click the Design button in the action bar to enter the editor.
- Create an SQL Query by right-clicking on the SQL Query node in the 2D editor and selecting Add button.

- In this example, we set the name of this SQL Query to UpdateQuery.

- Database Connection: Select an item whose status is "Connected "in the "Databases" ->"Database Connection" list. Here we select the TestSQLQuery already created in Step 1.
- Query Type: In this example, we want to update the table data, so we choose Update Query.
- SQL Editor: Write the following SQL statement that adds a new row to the
person_managementtable with a parameter. Parameters: Create a parameter called age. Acts as a placeholder in an SQL statement to which you can pass concrete values when executing a query.
- Click the "Test" button.You can see that Result returns the data 1, which means that the execution was successful, affecting a row of data.
Note:Executing statements of type 'Update Query' via the test button will also actually modify the database contents.
Use Update Query¶
- In the Design Page Tools window, add 4 Label, 2 Text input, 1 DropDown, 1 NumberInput, and 1 Button to the page.

Compose a simple Add data page as follows.

- Select the button control and click the icon pointed by the arrow to open the configuration page of the action.

- Configure the mouse pressed event for the button.Each time the button is clicked, get the values for the input and drop-down fields, and add the values to the database.
// Get name const nameValue = System.Page.getPropertyValue('nameInput#text') // Get email const emailValue = System.Page.getPropertyValue('emailInput#text') // Get gender const genderValue = System.Page.getPropertyValue('genderDropdown#selectedValue') // Get age const ageValue = System.Page.getPropertyValue('ageInput#value') // Return if any value is missing if (!nameValue || !emailValue || !genderValue || !ageValue) { return; } // Execute script const result = await System.Db.runSqlQuery('UpdateQuery', [ { name: 'name', value: nameValue }, { name: 'email', value: emailValue }, { name: 'gender', value: genderValue }, { name: 'age', value: ageValue }, ]) // If execution is successful, clear values if (result) { // Clear name System.Page.setPropertyValue('nameInput#text', '') // Clear email System.Page.setPropertyValue('emailInput#text', '') // Clear gender System.Page.setPropertyValue('genderDropdown#selectedValue', 'Male') // Clear age System.Page.setPropertyValue('ageInput#value', '') // Refresh table data const table = await System.UI.findControl('Table2') table.reload() } - Click the preview button on the page, and press the button on the preview page to add data to the database. When the new data is added, the table is reloaded and the new data is displayed.