Query¶
Example¶
According to the age entered by the user, the corresponding person is queried in the database, and the query result is displayed through the table.
Steps¶
Creating a database connection¶
On the "Databases"->"Database Connection" page, create a new database connection named TestSQLQuery.

There is a table named person_management in the database, which is used to store personnel information.
Its structure is as follows:
| Id | name | gender | age | |
|---|---|---|---|---|
| 1 | Alice Johnson | [email protected] | Female | 18 |
| 2 | Bob Smith | [email protected] | Male | 19 |
| 3 | Charlie Brown | [email protected] | Male | 19 |
| 4 | Diana White | [email protected] | Female | 18 |
| 5 | Edward Green | [email protected] | Female | 20 |
Create SQL Query¶
- Create the project, click the Design button in the action bar to enter the editor.
- Create an SQL Query by right-clicking on the SQL Query node in the 2D editor and selecting Add button.

- In this example, we set the name of this SQL Query to Query.

- Database Connection: Select an item whose status is "Connected "in the "Databases" ->"Database Connection" list. Here we select the TestSQLQuery already created in Step 1.
- Query Type: Select Query.
- SQL Editor: Write the following query that searches the
person_managementtable against the value of age. Where "age" denotes the parameter. - Parameters: Create a parameter called age. Acts as a placeholder in an SQL statement to which you can pass concrete values when executing a query.
- Click the "Test" button to see the results.

Use Query¶
- Find the Table control in the Tools window of the 2D design page and drag it to the page.

- Select the table control, in the property bar, click the binding button of the "Table" property, and bind an SQL Query for it.

- After selecting SQL Query, choose the newly created query "Query" from the Name dropdown list.

- Click the bind button for the parameter "age".
The property binding window pops up and binds it to the value property of NumberInput1. When NumberInput1 enters different values, the query is performed according to different ages. 
- Transform allow you to add, modify, or remove columns from the query again. When the Test button is clicked, the result is as follows:
If we want to hide the id column, we can write the following script in the transformation. - Click the Test button again.In the results list, the id column is no longer displayed.

- Finally, we want to make sure that polling mode is set to off. This means that the query will not run continuously, but only when the parameters change, such as when a new value is entered inside NumberInput1.

- Click the "OK" button to finish binding, and click the preview of the page for testing. Enter the age to query in the " NumberInput1" of the preview screen to retrieve the matching data and display the query results in the table.