Skip to content

Read/Write Mode Bindings

Read/Write Mode binding refers to the automatic synchronization between a control's property and a tag, dynamic tag, or another property.

This means when the data source changes, the control's style or value updates automatically; when the user modifies the control's style or value, the data source is also updated automatically.

Controls and Properties that Support Read/Write Mode Binding

Control Property
Text Input Text
Number Input Value
Slider Value
Checkbox Selected
Radio Button Selected Text/Selected Value
Dropdown Selected Text/Selected Value
Datetime Input Date

Tag Bindings with Read/Write Mode

In the property binding window, after selecting a tag, you can enable the "Read/Write Mode" option. When enabled, a fallback option can be set — if the write operation fails, the value will revert to the last valid value.

alt text

Example

The number input control and tag are configured with Read/Write Mode binding.

  1. Draw a number input control on the page.
  2. Click the bind button on the "Value" property of the control.

    alt text

  3. After selecting the tag in the "Property Binding" window, check the "Read/Write Mode" checkbox and click the "OK" button to complete the binding.

    alt text

  4. On the running page, when the value of the tag changes, the value displayed in the number input control changes synchronously; clicking the Enter key after entering the value in the number input control will write the entered value back to the bound tag.

Property Bindings with Read/Write Mode

In the property binding window, after selecting a property, you can enable the "Read/Write Mode" option. When enabled, a fallback option can be set — if the write operation fails, the value will revert to the last valid value.

alt text

Example

The number input and slider are configured with Read/Write Mode binding.

  1. Draw a number input and a slider control on the page.
  2. Click the bind button of the "Value" property of the number input.

    alt text

  3. In the "Property Binding" window, select the value property of the slider, check the "Read/Write Mode" checkbox, and click the "OK" button to complete the binding.

    alt text

  4. On the running page, when the value of the slide changes, the value displayed in the number input changes synchronously; when you enter a value in the number input and click the Enter key, the value of the slide changes accordingly.

    bidirectional

Dynamic Tag Bindings with Read/Write Mode

In the property binding window, after selecting a dynamic tag, you can enable the "Read/Write Mode" option. When enabled, a fallback option can be set — if the write operation fails, the value will revert to the last valid value.

alt text

Example

The text input is bound to an dynamic tag to display the running status of different motors. When a different motor is selected in the drop-down box, the running status of the motor is displayed in the text input, and the running status of the motor can be modified.

  1. Draw a text input, a dropdown, and 2 text label controls on the page.

    alt text

  2. The dropdown options are set to: Motor 1, Motor 2, Motor 3.

  3. Click the bind button of the "Text" property of the text input control.

    alt text

  4. After selecting "Dynamic Tag" in the property binding window, configure the required settings, check the "Read/Write Mode" checkbox, and click the "OK" button to complete the binding.

    alt text

  5. On the running page, when the options in the dropdown change, the value of the text input changes. When Motor 1 is selected, the text input displays the running status of Motor 1, and when Motor 2 is selected, the text input displays the running status of Motor 2.

  6. Entering true or false in the text input and clicking the Enter key will modify the operating status of the currently selected motor.