Datetime Input¶
The Datetime Input control is used to set the date and format the date.

Properties
| Name | Description |
|---|---|
| Name | The name of this control. |
| X | Distance of the left side of the control from the left side of the canvas. |
| Y | The distance from the top of the control to the top of the canvas. |
| W | Width of the control. |
| H | The height of the control. |
| Date | Sets the date displayed on the control. |
| Picker Type | Sets the format of the content displayed by the control, which contains Datetime and Date. When Datetime is selected, the year, month, day, hour, minute and second can be selected on the control; When Date is selected, only the year, month and day can be selected. ![]() |
| Format | Format the date, you can drop down to select the preset format, or you can input your own. Click to bring up the Format pop-up window, and double-click in the pop-up window to select the format. |
| Background | The background color of the control. ![]() |
| Picker Background | The background color of the control's popup calendar window. ![]() |
| Border Color | The border color of the control. |
| Border Thickness | The border thickness of the control. |
| Font | Sets the font of the control. This includes font , font size, font color, bold, and italic. |
Event
Allows you to perform a specific event based on certain conditions. See the Event page for a complete description of the various events.
Example
Display the current system time with the Datetime Input control.

- Insert a Datetime Input control on the page.
- Set the following properties for the control.
| Property | Value |
|---|---|
| Background | 03172c |
| Calendar Background | eff0f2 |
| Border Color | 12b5ac |
| Border Thickness | 2 |
| Fonts | Digital Numbers, 18, bold, font color: 12b5ac |
| Picker Type | Datetime |
| Formatting | a h:mm:ss |
3.Set event for the control, event type is "LifeCycle" -> "Loaded".
4.Turn on the "Enable" button and enter the following script into the Script Editor:
const data = await System.Tag.read('@System:Server.CurrentDateTime')
const calendar = await System.UI.findControl('DatetimeInput1');
calendar.value = data.value;
calendar.applyChanges();

Click to bring up the Format pop-up window, and double-click in the pop-up window to select the format.