Skip to content

Alarm Acknowledge

After the alarm occurs, the alarm can be acknowledged. There are three acknowledge modes, which are configured in the alarm attributes of the tag window.

  • Automatic
  • Manual (Comment Required)
  • Manual (No Comment)

Acknowledge Mode

In the alarm configuration of the tag, set the Ack Mode for the alarm.

alt text

Automatic

After the alarm is generated, if it returns to normal value later, the system automatically acknowledges this alarm. Once automatically acknowledged, the alarm disappears from the real-time alarm control. Automatically acknowledged alarms can also be manually acknowledged at any time before the alarm returns to normal value.

Manual (Comment Required)

After the alarm is generated, it must be confirmed manually.And enter the confirmation information. Otherwise, even if the current alarm has returned to normal, it will not disappear from the real-time alarm control.

After selecting the alarm, click the confirmation button, and the confirmation window will pop up. After entering the confirmation information, the confirmation will be completed. After confirmation, the alarm disappears from the real-time alarm control.

alt text

Manual (No Comment)

After the alarm is generated, it must be confirmed manually, otherwise even if the current alarm has returned to normal, it will not disappear from the real-time alarm control.

After selecting the alarm, click the confirmation button to complete the confirmation. After confirmation, the alarm disappears from the real-time alarm control.

alt text

How to Ackonwledge

  1. On the real-time alarm control, after checking the alarm, click the “Acknowledge” button at the bottom right corner of the control to acknowledge it.

    alt text

  2. Acknowledge by clicking directly on the "Priority" button.

    alt text